:DISPlay:MDISplay:DOCK
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
Command Syntax
:MDISplay:DOCK {ON | OFF | 1 | 0}
Query Syntax
:MDISplay:DOCK?
Query Response
{1 | 0}
Description
Turns on or off the docking of the message area located on the bottom of the display. Turning docking on prevents messages from hiding any portion of the graticule. When docking is turned off, the graticule's height is increased by a small amount. The default setting is OFF.