:MEASure:RESPonse:AVERage?
Flex Apps:
FlexPLL
Query Syntax
:MEASure:RESPonse:AVERage?
Description
Returns the current value for Response's Average measurement. This is the average amplitude of the Response plot.
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':MEASure:RESPonse:AVERage:STATus?')):
measurement = Flex.query(':MEASure:RESPonse:AVERage?')
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.