Response Commands
Flex Apps:
FlexPLL
Use the :MEASure:RESPonse commands to return the scalar Response and Response (Model) measurements that are shown in FlexPLL's results table. The table is displayed just below the graph as seen in the following picture. To return Memory and Memory (Model) measurements, use the :MEASure:RMEMory commands.
Before you can return a scalar measurement, you must first display the measurements using the :RESPonse subsystem's :RESPonse:DISPlay command. For the Average, Minimum, and Maximum flatness measurements you must additionally turn on their display using the :RESPonse subsystem's :RESPonse:FLATness:MEASure:DISPlay command.