:MEASure:RESPonse:TDENsity:STATus:REASon?
Flex Apps:
FlexPLL
Query Syntax
:MEASure:RESPonse:TDENsity:STATus:REASon?
Description
Returns a string that explains the reason for a failed :MEASure:RESPonse:TDENsity: measurement. If the measurement was successful, a null string is returned. Use the STATus? query to determine if the measurement has failed.