:MEASure:RMEMory:AVERage:STATus?
Flex Apps:
FlexDCA
FlexPLL
Query Syntax
:MEASure:RMEMory:AVERage:STATus?
Description
Queries the status of the :MEASure:RMEMory:AVERage measurement. Use the :MEASure:RMEMory:AVERage:STATus:REASon? child query to determine the reason for a invalid or questionable measurement.
The query response is:
{CORR | INV | QUES}
CORR- The measurement result is correct.
INV- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
QUES- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.