Memory Commands
Flex Apps:
FlexPLL
Use the :MEASure:RMEMory commands to return the scalar Memory and Memory (Model) measurements that are shown in FlexPLL's results table. The table is displayed just below the graph as seen in the following picture. To return Response and Response (Model) measurements, use the :MEASure:RESPonse commands.
Before you can return a scalar measurement, you must first display the measurements using the :RMEMory subsystem's :RMEMory:DISPlay command. For the Average, Minimum, and Maximum flatness measurements you must additionally turn on their display using the :RMEMory subsystem's :RMEMory:FLATness:MEASure:DISPlay command.