:MEASure:RMEMory:BANDwidth:STATus:REASon?
Flex Apps:
FlexPLL
Query Syntax
:MEASure:RMEMoryN:BANDwidth:STATus:REASon?
Where N identifies one of four {1:4} possible JTF response memories. For example, :MEASure:RMEMory3.
Description
Returns a string that explains the reason for a failed :MEASure:RMEMory:BANDwidth measurement. If the measurement was successful, a null string is returned. Use the :MEASure:RMEMory:BANDwidth:STATus? query to determine if the measurement has failed.