Measurement History Tab
Starting with PD1000A Control Software version 2022.321 (or later), all tests are recorded and available in the Measurement History screen.
Additional Features of the Measurement History
Measurement History
System State Column
Test completed without errors. Test completed but with a warning. Warning messages are recorded in the Measurement History. Errors occurred during the test execution or data extraction. Error messages are recorded in the Measurement History. Test aborted by user, message recorded in Measurement History. No icons means that the selected test was done on a previous version of the PD1000A Control software. These are not available for Run Extraction(s)....
The other columns in the Measurement History table are taken directly from the main test parameter screen.
You can reorder the columns by holding the left mouse key down on a column head and sliding it to the position you want.
Using Filters
- Click the Add Filter tab.This adds a SystemState filter menu to the screen. Click the down arrow to open the list of filter types; scroll down for the complete list.
- Click the down arrow next to Equals to select the type of filter to use.
- Enter the parameter in the blank field.
- Click Apply Filters.
For example, if you want a list of all measurements made at 200 volts or greater:
To remove a filter from the list, select the filter to remove (click at the far left, the filter is highlighted when it is selected). Then click Remove selected Filter.
Reload Measurement History
This reloads the complete Measurement History. For example, after you delete one or more files or set and apply filters, then remove the filters and click Reload Measurement History to get the complete list of tests.
Additional Features of the Measurement History
Click on any test to highlight it; right click to open the Context menu. Use the Shift or Ctrl keys to select multiple tests.
Load Measurement(s)...
Select one or more tests from the Measurement History tab, right click to highlight the context menu, select Load Measurement(s)... from the context menu to open the Results tab. Then click on the Selected Result down arrow to select one of the test results.
Run Extraction(s)...
Run Extraction(s)... allows you to open previous DPT measurement results in the Infiniium Offline PC-Based Oscilloscope Analysis Software (Version 06.50.xxxxx and all previous versions have been tested and work without problems. Do not use version 06.60.00403.) for evaluation. For example, you may want to expand the Turn-On / Turn-Off switching times on the oscilloscope display or change the IEC 10%/90% measurement points. The Offline software allows you to view, analyze, share, and document previously captured DPT measurements.
To run extractions, the Infiniium Oscilloscope Offline software must be running first; Run Extraction(s)... does not open or start the Infiniium Oscilloscope software. Only one instance of the Infiniium can run at a time.
Run Extraction(s)... is available only for Double-Pulse Tests run with PD1000A Control Software version 2023.324 (or later).
To use Run Extraction(s)...:
- Start the Infiniium Oscilloscope Offline software on the same PC as the PD1000A Control software.
- In Measurement History view, right click on the DPT test you want to analyze.
- Click on Run Extraction(s)....
- The PD1000A Control software reruns the analysis and transfers the measurement results to the Offline software.
A list of extractions you performed is available in the Results tab under Selected Extractions. You can do multiple extractions on one file; this list allows you to switch between the extractions.
It is beyond the scope of this manual to describe how to use the Infiniium Offline PC-Based Oscilloscope Analysis Software. Refer to the Offline Software help file.
Select Columns
This allows you to select and delete columns from the Measurement History.
Change Model ID
The Model ID is part of the Output Directory path (see “Global Settings in "Settings Drop-Down Menu”) for saving test measurement data. Changing the Model ID moves the measurement on the hard disk to correspond to a new measurement path.
Right click the test that you want to change the Model ID. The context menu opens with the model ID of the test you selected. Type in the new Model ID and click Change.... The control software creates a new folder with the new Model ID name.
Delete a Measurement from the Measurement History
To delete a test from the Measurement History, delete the measurement from the output folder. The next time the Measurement History is loaded (or click Reload Measurement History) the test does not appear in the Measurement History.
Top