Measurement Results Screens
                                        Depending on the type of test (Standard, Clamp, or Reverse Recovery, PD1550A does not support Clamp measurements) and the extractions selected (Extract Switching Characteristics, Extract Switching Locus, Enable Screenshots, etc), the Results Tab shows the measured or calculated results of the DPT test. These results include an oscilloscope capture, Gate Charge, Test Parameters, etc.
                                        
                                            
                                                
                                            
                                        
                                        Selected Result
                                        Shows the measured or calculated results of the DPT test. Note that you can select one or more tests from the Measurement History tab, right click, select Load Measurement(s)... to open the Results tab. Then click on the Selected Result down arrow to select one of the test results.
                                        Selected Extractions
                                        Provides a list of the Run Extraction(s) you have performed. You can do multiple extractions on one file; this list allows you to switch between the extractions.
                                        Comment Field on each Results Page
                                        Comments fields at the bottom of each Results page (Oscilloscope Capture, Gate Charge, Signal Levels and Time, etc.) are automatically saved.
                                        Test Results Screens
                                        The following test result screens are available after running Double-Pulse Tests (DPT). Not every screen is shown for every test; the screens displayed depend on the type of test run and the selected data extractions. 
                                        For definitions of terms, see Double-Pulse Test Terms and Definitions.
                                        Note that you can use the mouse roller and arrow keys (on your keyboard) to zoom in on the oscilloscope waveforms.
                                         
                                        
                                         
                                        
Top
                                        
                                        Standard Double-Pulse Tests:
                                        
                                            - Gate Charge Results
Displayed only after a Standard DPT, these are the Gate Charge Waveforms and actual measured values. For example:
               
              				QG = Total Gate Charge,
						               QGD
						= Gate Drain Charge
               QGS(PL) = Plateau Gate Charge
                                             
                                            - IV Curves
Displayed only after a Standard DPT, the IV Curve Waveform (IDS vs. VGS) for the device. For example:
               
                                             
                                            - IV Derivation
Displayed only after a Standard DPT, these are the IV Derivation points (IDS vs. VDS) for the device. For example:
               
                                             
                                            - IV Single Curves
Displayed only after a Standard DPT, these are the IDS vs. VGS curves and measurement results for the device. For example:
               
                                             
                                            - Standard Oscilloscope Capture
Displayed only after a Standard DPT, this is the oscilloscope waveform capture for the device. For example:
               
                                             
                                            - Standard Parameters
Displayed only after a Standard DPT, these are the test parameters that you set for the test and the actual measured results. For example:
              
 
					
              First Pulse Width is the time that IDS is ramping up. This is calculated by the software based on the measurement parameters you specify.
                                             
                                            - Signal Levels and Times
Displayed only after a Standard DPT, this is the measured signal levels and measurement time for the test. For example:
               
Note: High Times and Low Times are for the respective measurement signals (Gate Control Signal, Output Voltage, or Output Current). High Times refer to the 90% and Low Times refer to the 10% levels of the signals. As part of the extraction process, the DPT analysis software determines the minimum (0%) and maximum (100%) levels of the signals. Then it looks for the times where the signals cross 10% and 90%. The 10% and 90% times are used to extract the actual switching characteristics.
See also: Turn-On and Turn-Off Characteristics.
                                             
                                            - Switching Characteristics
Displayed only after a Standard DPT, these are the switching characteristics measured or calculated from the test. For example:
               
               See also: Turn-On and Turn-Off Characteristics.
               Note: Integration Time and Tail time are measured only for IGBT devices. For FET devices, they will show NaN (Not a Number). Total Switching Energy is the sum of Turn On Energy and Turn Off Energy.
                                             
                                            - Switching Locus
Displayed only after a Standard DPT, this is the Switching Locus curves for the device. For example:
               
                                             
                                        
                                         
                                        
Top
                                        
                                        Standard Sweep Tests
                                        
                                        
Top
                                        
                                        Clamp Double-Pulse Tests (not supported in PD1550A):
                                        
                                            - Clamp Parameters
Displayed only after a Clamp DPT, these are the parameters you set for the Clamp  Test and the actual measured values. For example:
                
                                             
                                            - Clamp RdsOn
Displayed only after a Clamp DPT, these are the actual measured values. For example:
               
 
                                             
                                            - Clamp Oscilloscope Capture
Displayed only after a Clamp DPT, this displays the oscilloscope waveform capture for the test. For example:
               
                                             
                                        
                                        
Top
                                        
                                        Reverse Recovery Double-Pulse Tests:
                                        
                                            - Reverse Recovery
Displayed only after a Reverse Recovery DPT,  these are the actual measured values for the test. For example: 
               
                                             
                                            - Reverse Recovery  Parameters
Displayed only after a Reverse Recovery DPT,  these are the parameters you set for the Reverse Test and the actual measured values. For example: 
               
                                             
                                            - Reverse Recovery Oscilloscope Capture
Displayed only after a Reverse Recovery DPT, this displays the oscilloscope waveform capture for the test. For example:
               
                                             
                                        
                                        
Top