IFormattedIO488::FlushRead
Description
Flushes the contents of the read buffer until an end condition is reached.
VB Prototype
FlushRead(
)
C++ Prototype
HRESULT FlushRead(
);
Return Value
Refer to the table of return codes.
See Also
IO, InstrumentBigEndian, WriteString, WriteNumber, WriteList, WriteIEEEBlock, ReadString, ReadNumber, ReadList, ReadIEEEBlock, FlushWrite, FlushRead, SetBufferSize, IFormattedIO488 Overview