IFormattedIO488::ReadString

Description

Reads from the read buffer until an end condition is reached (termination character, END signal, etc), and returns the data in a string.

VB Prototype

value As String = ReadString(
)

C++ Prototype

HRESULT ReadString(
  BSTR* pData
);

Parameters

pData

The string data retrieved from the read buffer.

Return Value

Refer to the table of return codes.

See Also

IO, InstrumentBigEndian, WriteString, WriteNumber, WriteList, WriteIEEEBlock, ReadString, ReadNumber, ReadList, ReadIEEEBlock, FlushWrite, FlushRead, SetBufferSize, IFormattedIO488 Overview