IFormattedIO488::SetBufferSize

Description

Sets the size of the read, write, or both formatted I/O buffers.

VB Prototype

SetBufferSize(
  mask As BufferMask,
  size As Long
)

C++ Prototype

HRESULT SetBufferSize(
  BufferMask mask,
  long size
);

Parameters

mask

Which buffer to resize.

size

The new buffer size.

Return Value

Refer to the table of return codes.

See Also

IO, InstrumentBigEndian, WriteString, WriteNumber, WriteList, WriteIEEEBlock, ReadString, ReadNumber, ReadList, ReadIEEEBlock, FlushWrite, FlushRead, SetBufferSize, IFormattedIO488 Overview