IFormattedIO488::InstrumentBigEndian
Description
Affects the behavior of the Read/WriteIEEEBlock methods:These methods interpret the binary data as Big-Endian or Little-Endian based on this property.
VB Prototype
Dim value As Boolean
value = object.InstrumentBigEndian
object.InstrumentBigEndian = value
C++ Prototype
HRESULT get_InstrumentBigEndian(
VARIANT_BOOL* InstrumentBigEndian
);
HRESULT put_InstrumentBigEndian(
VARIANT_BOOL InstrumentBigEndian
);
Return Value
Refer to the table of return codes.
See Also
IO, InstrumentBigEndian, WriteString, WriteNumber, WriteList, WriteIEEEBlock, ReadString, ReadNumber, ReadList, ReadIEEEBlock, FlushWrite, FlushRead, SetBufferSize, IFormattedIO488 Overview