IRegister::DestinationBigEndian

Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.

Description

Indicates whether the destination address space uses Big Endian or Little Endian byte order.

VB Prototype

Dim value As Boolean
value = object.DestinationBigEndian

object.DestinationBigEndian = value

C++ Prototype

HRESULT get_DestinationBigEndian(
  VARIANT_BOOL* DestinationBigEndian
);

HRESULT put_DestinationBigEndian(
  VARIANT_BOOL DestinationBigEndian
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, DestinationBigEndian, DestinationIncrement, SourceBigEndian, SourceIncrement, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, In8, In16, In32, Out8, Out16, Out32, MoveIn8, MoveIn16, MoveIn32, MoveOut8, MoveOut16, MoveOut32, Move, IRegister Overview