IRegister::Move
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
Moves data from the specified source to the specified destination. The source and the destination can either be local memory or the offset of the interface with which this INSTR or MEMACC resource is associated. This operation uses the specified data width and address space.
If the session object is an INSTR session, the offset parameters specify relative offsets from the start of the instrument's address space. If
session object is a MEMACC session, the offset parameters are absolute offsets from the start of memory in the specified VXI address space.
VB Prototype
Move(
srcSpace As Short,
srcOffset As Long,
srcWidth As DataWidth,
destSpace As Short,
destOffset As Long,
destWidth As DataWidth,
length As Long
)
C++ Prototype
HRESULT Move(
short srcSpace,
long srcOffset,
DataWidth srcWidth,
short destSpace,
long destOffset,
DataWidth destWidth,
long length
);
Parameters
srcSpace
Specifies the address space of the source.
The following values are legal:
| VXI_A16_SPACE | Address the A16 address space of VXI/MXI bus. |
| VXI_A24_SPACE | Address the A24 address space of VXI/MXI bus. |
| VXI_A32_SPACE | Address the A32 address space of VXI/MXI bus. |
srcOffset
Offset (in bytes) of the address or register from which to read.
srcWidth
Specifies the data width of the source.
destSpace
Specifies the address space of the destination.
The following values are legal:
| VXI_A16_SPACE | Address the A16 address space of VXI/MXI bus. |
| VXI_A24_SPACE | Address the A24 address space of VXI/MXI bus. |
| VXI_A32_SPACE | Address the A32 address space of VXI/MXI bus. |
destOffset
Offset (in bytes) of the starting address or register to which to write.
destWidth
Specifies the data width of the destination.
length
Number of elements to transfer, where the data width of the elements to transfer is identical to the source data width.
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, DestinationBigEndian, DestinationIncrement, SourceBigEndian, SourceIncrement, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, In8, In16, In32, Out8, Out16, Out32, MoveIn8, MoveIn16, MoveIn32, MoveOut8, MoveOut16, MoveOut32, Move, IRegister Overview