IRegister::DestinationIncrement

Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.

Description

Used by the MoveOut functions to determine whether to do a block move or a FIFO read.

VB Prototype

Dim value As Long
value = object.DestinationIncrement

object.DestinationIncrement = value

C++ Prototype

HRESULT get_DestinationIncrement(
  long* DestinationIncrement
);

HRESULT put_DestinationIncrement(
  long DestinationIncrement
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, DestinationBigEndian, DestinationIncrement, SourceBigEndian, SourceIncrement, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, In8, In16, In32, Out8, Out16, Out32, MoveIn8, MoveIn16, MoveIn32, MoveOut8, MoveOut16, MoveOut32, Move, IRegister Overview