IRegister::GetAttribute

Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.

Description

Use of this method is discouraged. All the non-deprecated standard attributes are accessible via properties on the appropriate COM interfaces.

VB Prototype

value As Variant = GetAttribute(
  attribute As Long
)

C++ Prototype

HRESULT GetAttribute(
  long attribute,
  VARIANT* pAttrState
);

Parameters

attribute

The attribute type to retrieve.

pAttrState

The value of the attribute.

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, DestinationBigEndian, DestinationIncrement, SourceBigEndian, SourceIncrement, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, In8, In16, In32, Out8, Out16, Out32, MoveIn8, MoveIn16, MoveIn32, MoveOut8, MoveOut16, MoveOut32, Move, IRegister Overview