IResourceManager3::FindRsrc
Description
This method uses VISA search strings to find VISA resources. For example, GPIB?* will find all GPIB resources the Resource Manager knows about; ASRL?* will find all serial resources. GPIB0::?* will find all resources on GPIB0.
VB Prototype
value As 
				SAFEARRAY (BSTR)= FindRsrc(
                                        
  expr As String
)
	
C++ Prototype
HRESULT FindRsrc(
                                        
  BSTR expr,
  SAFEARRAY(BSTR)* pFindList
);
	
Parameters
expr
The Search String.
pFindList
The list of resources matching the search string.
Return Value
Refer to the table of return codes.
See Also
SoftwareManufacturerName, SoftwareManufacturerID, Description, ComponentVersion, ProgID, SpecVersion, FindRsrc, Open, ParseRsrc, ParseRsrcEx, IResourceManager3 Overview