IResourceManager3::ProgID
Description
The programmatic ID that can be used by COM to create this object.
VB Prototype
Dim value As Stringvalue = object.ProgID
C++ Prototype
HRESULT get_ProgID(
                                        
  BSTR* ProgID
);
		
Return Value
Refer to the table of return codes.
See Also
SoftwareManufacturerName, SoftwareManufacturerID, Description, ComponentVersion, ProgID, SpecVersion, FindRsrc, Open, ParseRsrc, ParseRsrcEx, IResourceManager3 Overview