IResourceManager3::ParseRsrc
Description
This operation parses a resource string to verify its validity. It should succeed for all strings returned by FindRsrc and recognized by Open. This operation is useful if you want to know what interface a given resource descriptor would use without actually opening a session to it.
VB Prototype
ParseRsrc(
                                        
  ResourceName As String,
  pInterfaceType As Short,
  pInterfaceNumber As Short,
  pSessionType As String
)
	
C++ Prototype
HRESULT ParseRsrc(
                                        
  BSTR ResourceName,
  short* pInterfaceType,
  short* pInterfaceNumber,
  BSTR* pSessionType
);
	
Parameters
ResourceName
The VISA address string.
pInterfaceType
The interface type number of the resource.
pInterfaceNumber
The interface number of the resource.
pSessionType
The session type of the resource.
Return Value
Refer to the table of return codes.
See Also
SoftwareManufacturerName, SoftwareManufacturerID, Description, ComponentVersion, ProgID, SpecVersion, FindRsrc, Open, ParseRsrc, ParseRsrcEx, IResourceManager3 Overview