IResourceManager3::SpecVersion

Description

The VISA-defined version information for the specification version this component complies to.

VB Prototype

Dim value As Long
value = object.SpecVersion

C++ Prototype

HRESULT get_SpecVersion(
  long* SpecVersion
);

Return Value

Refer to the table of return codes.

See Also

SoftwareManufacturerName, SoftwareManufacturerID, Description, ComponentVersion, ProgID, SpecVersion, FindRsrc, Open, ParseRsrc, ParseRsrcEx, IResourceManager3 Overview