IVxi::FastDataChannel
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
Determines which FDC channel will be used to transfer the buffer.
VB Prototype
Dim value As Short
                                            value = object.FastDataChannel
                                        
object.FastDataChannel = value 
                                        
C++ Prototype
HRESULT get_FastDataChannel(
                                        
  short* FastDataChannel
);
		
HRESULT put_FastDataChannel(
                                        
  short FastDataChannel
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, CommanderLA, DestinationAccessPrivilege, DeviceClass, FastDataChannel, FastDataChannelMode, FastDataChannelUsePair, ImmediateServant, LogicalAddress, MainframeLogicalAddress, ManufacturerID, ManufacturerName, MemoryBase, MemorySize, MemorySpace, ModelCode, ModelName, TriggerID, Slot, SourceAccessPrivilege, TriggerSupport, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, CommandQuery, IVxi Overview