IVxi::HardwareInterfaceNumber
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
The board number of the hardware interface.
VB Prototype
Dim value As Short
                                            value = object.HardwareInterfaceNumber
                                        
C++ Prototype
HRESULT get_HardwareInterfaceNumber(
                                        
  short* HardwareInterfaceNumber
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, CommanderLA, DestinationAccessPrivilege, DeviceClass, FastDataChannel, FastDataChannelMode, FastDataChannelUsePair, ImmediateServant, LogicalAddress, MainframeLogicalAddress, ManufacturerID, ManufacturerName, MemoryBase, MemorySize, MemorySpace, ModelCode, ModelName, TriggerID, Slot, SourceAccessPrivilege, TriggerSupport, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, CommandQuery, IVxi Overview