IVxi::FastDataChannelMode
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
Determines which FDC mode to use (Normal mode or Stream mode).
VB Prototype
Dim value As FDCMode
                                            value = object.FastDataChannelMode
                                        
object.FastDataChannelMode = value 
                                        
C++ Prototype
HRESULT get_FastDataChannelMode(
                                        
  FDCMode* FastDataChannelMode
);
		
HRESULT put_FastDataChannelMode(
                                        
  FDCMode FastDataChannelMode
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, CommanderLA, DestinationAccessPrivilege, DeviceClass, FastDataChannel, FastDataChannelMode, FastDataChannelUsePair, ImmediateServant, LogicalAddress, MainframeLogicalAddress, ManufacturerID, ManufacturerName, MemoryBase, MemorySize, MemorySpace, ModelCode, ModelName, TriggerID, Slot, SourceAccessPrivilege, TriggerSupport, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, CommandQuery, IVxi Overview