IVxi::FastDataChannelUsePair
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
If set to true, a channel pair will be used for transferring data. Otherwise, only one channel will be used.
VB Prototype
Dim value As Boolean
                                            value = object.FastDataChannelUsePair
                                        
object.FastDataChannelUsePair = value 
                                        
C++ Prototype
HRESULT get_FastDataChannelUsePair(
                                        
  VARIANT_BOOL* FastDataChannelUsePair
);
		
HRESULT put_FastDataChannelUsePair(
                                        
  VARIANT_BOOL FastDataChannelUsePair
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, CommanderLA, DestinationAccessPrivilege, DeviceClass, FastDataChannel, FastDataChannelMode, FastDataChannelUsePair, ImmediateServant, LogicalAddress, MainframeLogicalAddress, ManufacturerID, ManufacturerName, MemoryBase, MemorySize, MemorySpace, ModelCode, ModelName, TriggerID, Slot, SourceAccessPrivilege, TriggerSupport, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, CommandQuery, IVxi Overview