| Ivi.Visa Namespace : IMessageBasedSession Interface |
For a list of all members of this type, see IMessageBasedSession members.
| Name | Description | |
|---|---|---|
![]() | EventQueueCapacity | The capacity of the event queue - the maximum number of pending events. (Inherited from Ivi.Visa.IVisaSession) |
![]() | FormattedIO | A reference to the formatted I/O interface. |
![]() | HardwareInterfaceName | Human readable text that describes the hardware interface. (Inherited from Ivi.Visa.IVisaSession) |
![]() | HardwareInterfaceNumber | The board number of the hardware interface. (Inherited from Ivi.Visa.IVisaSession) |
![]() | HardwareInterfaceType | Specifies the hardware interface type (GPIB, ASRL, etc.). (Inherited from Ivi.Visa.IVisaSession) |
![]() | IOProtocol | The protocol type for I/O communication with the physical resource. In some cases you may not be able to change the protocol, so reading this property value may not return the same value that was set. |
![]() | RawIO | A reference to the raw I/O interface. |
![]() | ResourceClass | The class of resource for this session (INSTR, INTFC, etc.). (Inherited from Ivi.Visa.IVisaSession) |
![]() | ResourceImplementationVersion | The version of this VISA.NET implementation. (Inherited from Ivi.Visa.IVisaSession) |
![]() | ResourceLockState | The current lock state of the resource for this session. (Inherited from Ivi.Visa.IVisaSession) |
![]() | ResourceManufacturerId | The IVI identification number of the software vendor of this VISA.NET implementation. (Inherited from Ivi.Visa.IVisaSession) |
![]() | ResourceManufacturerName | The name of the software vendor that corresponds to the ResourceManufacturerId property. (Inherited from Ivi.Visa.IVisaSession) |
![]() | ResourceName | The VISA resource name of the currently open resource. This name is the canonical version of the resource name and therefore may vary from the resource descriptor used to open/initialize the resource. (Inherited from Ivi.Visa.IVisaSession) |
![]() | ResourceSpecificationVersion | The version of the VISA.NET specification that describes the functionality provided by this session. (Inherited from Ivi.Visa.IVisaSession) |
![]() | SendEndEnabled | Enables/disables sending the END signal on the last byte of a write. |
![]() | SynchronizeCallbacks | Specifies whether callbacks must be performed in a specific synchronization context. If false, the implementation is allowed to execute callbacks in any context. The default value is true. (Inherited from Ivi.Visa.IVisaSession) |
![]() | TerminationCharacter | The ASCII character used to end reading. |
![]() | TerminationCharacterEnabled | If true, reads end when a termination character is received. |
![]() | TimeoutMilliseconds | The I/O timeout in milliseconds for I/O communication on this resource session. If the timeout is VisaConstants.ImmediateTimeout (0), operations will never wait for the device to respond. If the timeout is VisaConstants.InfiniteTimeout (-1), I/O communication will not timeout. (Inherited from Ivi.Visa.IVisaSession) |