IGpib::RepeatAddressingEnabled

Description

Specifies whether to use repeat addressing before each read or write operation.

VB Prototype

Dim value As Boolean
value = object.RepeatAddressingEnabled

object.RepeatAddressingEnabled = value

C++ Prototype

HRESULT get_RepeatAddressingEnabled(
  VARIANT_BOOL* RepeatAddressingEnabled
);

HRESULT put_RepeatAddressingEnabled(
  VARIANT_BOOL RepeatAddressingEnabled
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, PrimaryAddress, RENState, RepeatAddressingEnabled, SecondaryAddress, UnaddressingEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ControlREN, IGpib Overview