IGpib::SoftwareManufacturerName

Description

The name of the vendor of this software component.

VB Prototype

Dim value As String
value = object.SoftwareManufacturerName

C++ Prototype

HRESULT get_SoftwareManufacturerName(
  BSTR* SoftwareManufacturerName
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, PrimaryAddress, RENState, RepeatAddressingEnabled, SecondaryAddress, UnaddressingEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ControlREN, IGpib Overview