IGpib::Timeout

Description

The I/O timeout in milliseconds for I/O communication on this resource session.

VB Prototype

Dim value As Long
value = object.Timeout

object.Timeout = value

C++ Prototype

HRESULT get_Timeout(
  long* Timeout
);

HRESULT put_Timeout(
  long Timeout
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, PrimaryAddress, RENState, RepeatAddressingEnabled, SecondaryAddress, UnaddressingEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ControlREN, IGpib Overview