IGpib::UnaddressingEnabled
Description
Specifies whether to unaddress the device (UNT and UNL) after each read or write operation.
VB Prototype
Dim value As Boolean
value = object.UnaddressingEnabled
object.UnaddressingEnabled = value
C++ Prototype
HRESULT get_UnaddressingEnabled(
VARIANT_BOOL* UnaddressingEnabled
);
HRESULT put_UnaddressingEnabled(
VARIANT_BOOL UnaddressingEnabled
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, PrimaryAddress, RENState, RepeatAddressingEnabled, SecondaryAddress, UnaddressingEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ControlREN, IGpib Overview