N9048B Option NF2
|
|
For MXE N9038A and N9038B, this test is called Effective DANL Option NFE. For PXE N9048B, this test is called Effective DANL. |
Option NFE/NF2 provides noise corrections which will allow the EMI receiver to measure signals close to the noise. The corrections will essentially compensate for the known conversion loss of the EMI receiver RF front-end.
The noise floor improvement is inferred from amplitude measurements made on a signal close to the noise floor. The test is actually three measurements that are performed at each test frequency. The choice of test frequency was center of the band offset by 100 MHz times Pi. This frequency offset was done to avoid measuring residuals.
Measurement 1 (M1) — This is a DANL measurement made in a 300 kHz resolution bandwidth. The goal of this measurement is to baseline the noise of the DUT. The test signal amplitude will be placed approximately 5 dB above the measured noise floor.
Measurement 2 (M2) — The test signal amplitude is calculated from the DANL measurement. This step measures the amplitude of the test signal in the 30 Hz resolution bandwidth. The 30 Hz resolution bandwidth will provide a 40 dB improvement in SNR. The goal of this measurement is to baseline the true amplitude of the test signal.
Measurement 3 (M3) — The resolution bandwidth is set to 300 kHz and the amplitude of the signal (plus noise) is measured with the noise corrections set to On. The 300 kHz resolution bandwidth causes the SNR to be around 5 dB. The amplitude difference relative to the M2 measurement is the noise contribution.
The "effective noise, Neff" can be calculated from the results of these three measurements:
M1 = Uncorrected Noise (in watts) = N
M2 = Amplitude of signal with high SNR (in watts) = A
M3 = Amplitude of signal with low SNR (in watts) = A + Neff
Neff = A – (A + Neff)
Neff = M2 – M3
Let’s state this as a ratio because then we can easily calculate the relative improvement in terms of dB:
Noise Improvement (Linear) = Neff/N = (M2-M3)/M1
Noise Improvement (dB) = 10 x LOG(Neff/N) = 10 x LOG [(M2-M3)/M1]
The Effective DANL can be calculated by the following equation:
Effective DANL (dBm/Hz) = Uncorrected Noise (300 kHz RBW) + Noise Improvement (dB) + 1 Hz RBW Normalization
Effective DANL (dBm/Hz) = 10 x LOG(M1/.001) + 10 x LOG [(M2-M3)/M1] + 10 x LOG (300000)
Where: 10 x LOG (30000) normalizes the result to a 1 Hz resolution bandwidth.
For Option NFE, refer to the Effective DANL Adjustment.
If the Effective DANL test should fail, Option NF2 requires a manual noise floor characterization. To do this,
For PXE without WF1, press System > Alignments > Advanced > Characterize Noise Floor
For PXE with WF1, press System > Alignments > Advanced >Characterize EMI Receiver Noise Floor
Click here for troubleshooting.
|
Test Equipment |
Model Number1 |
|---|---|
|
Microwave Signal Generator #1 |
PSG Models |
|
BNC Cable |
8120-1840 |
|
Cable, 3.5 mm coaxial
|
11500E |
|
Cable, 2.4 mm coaxial
|
8120-6164 |
|
Adapter, 3.5 mm (f) to 3.5 mm (f)
|
83059B |
|
Adapter, Type-N (m) to 3.5 mm (f)
|
1250-1744 |
|
Adapter, Type-N (m) to 2.4 mm (f)
|
11903D |
|
Adapter, 2.4 mm (f) to 2.4 mm (f)
|
11900B |
|
Adapter, 2.4 mm (f) to 3.5 mm (f)
|
11901B |
|