N5241A/AS/B/BC, N5242A/AS/H85/B, N5244A/AS/B, N5245A/AS/B/BC, N5247A/AS/B/BC, N5249A/AS/B
|
|
Be sure that |
This topic shows the required equipment and connection setups for PNA models running the Factory Recommended Variant test plan. For more information about test plan variants, refer to the Test Plan Variants topic.
For test description, go to the topic's Overview page.
|
Test Equipment1 |
Recommended Model |
Alternate Model |
|
Signal Generator |
E8257D |
N5183B E8257C E8247C (not allowed for N5241x and N5242x PNA-X) |
|
Power meter |
N1914B |
N1914A |
|
PowerSensor 1, for 3.5 mm models |
U8485A2 Opt. 200 |
U8485A2 |
|
PowerSensor 1, for 2.4 mm models |
U8488A2 |
U8487A2 |
|
PowerSensor 1, for 1.85 mm models |
U8488A2 |
N8488A3 |
|
Dynamic Accuracy test set4 |
U3020BD01 |
U3020AD01 |
|
Load, 3.5 mm 50 W |
909D |
902C |
|
|
|
Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:
|
PNA models running the Factory Recommend Variant will use flexible power sensor channel assignment that will identify the channel that a power sensor is connected to using the ability of "smart" sensors such as the N848xA and U848xA series to report their full model and serial number. Therefore it is important to keep the power sensor on the channel where it was calibrated throughout the test procedures.
For more information about test plan variants, refer to the Test Plan Variants topic.