|
|
Be sure that |
This topic shows the required equipment and connection setups for PNA models using the Preferred Solution in the Normal Variant test plan. For more information about test plan variants, refer to the Test Plan Variants topic.
For test description, go to the topic's Overview page.
|
Test Equipment1 |
Recommended Model |
Alternate Model |
|
Signal Generator |
E8257D |
N5183B E8257C E8247C (not allowed for N5241x and N5242x PNA-X) |
|
Power meter |
N1914A |
E4419A/B |
|
PowerSensor LowFreq 1 |
N8482A |
N8482A-CFT |
|
Dynamic Accuracy test set2 |
U3020BD01 |
U3020AD01 |
|
Load, 3.5 mm 50 W |
909D |
902C |
|
|
|
Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:
|