|
|
|
This topic shows the required equipment and connection setups for PNA models running the Factory Recommended Variant test plan. For more information about test plan variants, refer to the Test Plan Variants topic.
For test description, go to the topic's Overview page.
Below is the required test equipment separated by the DUT connector type. Select the link that applies to the connector type for your PNA model.
N5241A/AS/B/BC, N5242A/AS/B, N5242AH85, N5249A/AS/B
N5221A/AS/B, N5222A/AS/B
N5231A/AS/B, N5232A/AS/B, N5239A/AS/B
N5230A/C with option 12x, 14x, 22x, 24x, or 02x
|
3.5 mm Connector Models |
||
|
Test Equipment1 |
Recommended Model |
Alternate Model |
|
Power meter |
N1914B |
N1914A |
|
PowerSensor 1 |
U8485A2 Option 200 |
U8485A2, 4 |
|
Gain Compression Test Set5 |
U3070BK01 |
U3070AK01 |
|
20 dB fixed attenuator, 3.5 mm For these models:
|
8493C Opt. 020 |
|
|
N5244A/AS/B, N5245A/AS/B/BC
N5224A/AS/B, N5225A/AS/B
N5234A/AS/B, N5235A/AS/B
N5230A/C with option 42x or 52x
|
2.4 mm Connector Models |
||
|
Test Equipment1 |
Recommended Model |
Alternate Model |
|
Power meter |
N1914B |
N1914A |
|
PowerSensor 1 |
U8488A2 |
U8487A2 |
|
PowerSensor 24
|
U8485A2 Option 200 |
|
|
Gain Compression Test Set5
|
U3070BK01 |
U3070AK01 |
|
20 dB fixed attenuator, 2.4 mm
|
8490D Opt. 020 |
|
|
N5247B/BC, N5227B
|
1.85 mm Connector Models |
||
|
Test Equipment1 |
Recommended Model |
Alternate Model |
|
Power meter |
N1914B |
N1914A |
|
PowerSensor 1 |
U8488A2 |
N8488A3 |
|
PowerSensor 24
|
U8485A2 Option 200 |
|
|
Gain Compression Test Set
|
U3070BK015 |
U3070AK015 |
|
20 dB fixed attenuator, 1.85 mm
|
8490G Opt. 020 |
Anritsu 41V-20 |
|
|
|
Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:
|
PNA models running the Factory Recommend Variant will use flexible power sensor channel assignment that will identify the channel that a power sensor is connected to using the ability of "smart" sensors such as the N848xA and U848xA series to report their full model and serial number. Therefore it is important to keep the power sensor on the channel where it was calibrated throughout the test procedures.
For more information about test plan variants, refer to the Test Plan Variants topic.
|
|
The Receiver Compression Above 50 GHz test will also test on the 50 GHz – 67 GHz ports of the test set. |
|
|
Notes for test process on the: N5242A/AS/B, N5244A/AS/B, N5245A/AS/B/BC, N5247A/AS/B/BC
|