This section lists the available performance tests for the PNA-L/X series network analyzers. Perform the tests in the order shown to minimize connection changes and to avoid recalibration of the power sensor. The tests to be performed and the test order depends on the model number.
There are now two test plan variants offered in the N7840A PNA Calibration Application: Factory Recommended Variant and Normal Variant. As of the E.20.00 release, all PNA models (except N5244/45AS with option H29) can use the Factory Recommended Variant test plan variant. The Factory Recommended Variant is the preferred variant as it optimizes connections for several tests and therefore reduces the overall test times.
PNA models with Low Frequency Extension (LFE) options and mm-Wave systems must use the Factory Recommended Variant.
The Factory Recommended Variant includes all tests from the Normal Variant test plan plus two new tests for LFE options:
For more information about test plan variants, refer to the Test Plan Variants topic page.
Click on the links below for the test list for your model.
mm-Wave Network Analyzer Systems Models:
N5290A, N5291A
|
|
These models can only run the Factory Recommended Variant test plan. |
Input VSWR (Option 090) a
SA Detector Accuracy (Option 090) a
Displayed Average Noise Level (Option 090) a
Also requires Option <RSA>. Refer to the test topic page for more information.
Only for models with option <SYN>.
PNA-X Models:
N5241A/AS/B/BC, N5242A/AS/B, N5242AH85, N5244A/AS/B, N5245A/AS/B/BC, N5247A/AS/B/BC, N5249A/AS/B
|
|
The following models are only supported in the Normal Variant — they cannot use the Factory Recommended Variant:
|
Receiver Compression at Low Frequency (LFE options)
Dynamic Accuracy at Low Frequency (LFE options)
Receiver Noise Figure (N5244A/AS/B, N5245A/AS/B/BC, N5247A/AS/B/BC Opt. 029/E29)
Receiver Noise Figure (26.5 GHz and below) (N5241A/AS/B/BC, N5242A/AS/B Opt. 029; and N5244AS, N5245AS Opt. H29)
System Default Cal Verification (Functional) Test (B/BC-models only)
Input VSWR (Option 090 only) d, e
SA Detector Accuracy (Requires Options 090 and <RSA>)
Displayed Average Noise Level (Requires Options 090 and <RSA>)
R-Channel Linearity (Option 561)
R-Channel Linearity Calibration (Option 560)
Noise Floor (Normal Variant only)
If a Z5623A H01 Dynamic Accuracy Test Set is used, an additional 30-minute wait can be avoided at the start of the test by connecting the power sensor to the test set at the completion of the Noise Floor test.
For the following models only:
N5244AS, N5245AS with Option H29
N524xB/BC models also require Option <RSA>. Refer to the test topic page for more information.
This test is called VSWR in the Normal Variant test plan.
Only for models with option <SYN>.
PNA Models:
N5221A/AS/B, N5222A/AS/B, N5224A/AS/B, N5225A/AS/B, N5227A/AS/B
Metrology Stability (Options 210, 410 only)
Receiver Compression at Low Frequency (LFE options)
Dynamic Accuracy at Low Frequency (LFE options)
System Default Cal Verification (Functional) Test (B-models only)
Input VSWR (Option 090 only) b, c
SA Detector Accuracy (Option 090 only) b
Displayed Average Noise Level (Option 090 only) b
Since three power sensors are required for frequency range above 50 GHz, the following tests are divided in TME to avoid unnecessary recalibration of the power sensors:
Noise Floor (Normal Variant only)
N522xB models also require Option <RSA>. Refer to the test topic page for more information.
This test is called VSWR in the Normal Variant test plan.
Only for models with option <SYN>.
PNA-L Models:
N5231A/AS/B, N5232A/AS/B, N5234A/AS/B, N5235A/AS/B, N5239A/AS/B
Receiver Compression at Low Frequency (N5231A/AS/B, N5232A/AS/B, N5239A/AS/B only)
System Default Cal Verification (Functional) Test (B-models only)
Input VSWR (Option 090 only) a, b
SA Detector Accuracy (Option 090 only) a
Displayed Average Noise Level (Option 090 only) a
N523xB models also require Option <RSA>. Refer to the test topic page for more information.
This test is called VSWR in the Normal Variant test plan.
N5230A, N5230C PNA-L Models
|
|
N5230A/C models with firmware version below A.07.00 cannot use the Factory Recommended Variant. |