N9933B/34B/35B/36B/37B/38B
The network analyzer used in certain tests must be calibrated with cables and adapters prior to running the test. The calibration will need to be repeated once every three days or if the adapters or cables have been disturbed. If it's been within the three day time-frame and the adapters and cables have not been disturbed, then the network analyzer calibration is not necessary and you may proceed with the test.
There are two calibration procedures used. These procedures are located in the Utilities Test Plan in TME. They are also embedded in the individual tests that require the network analyzer calibration procedure.
The following tests require this procedure:
The following tests require this procedure:
|
|
|
|
Test Equipment |
Recommended Model1 |
|---|---|
|
Optimized Test Station |
The Optimized Test Station consists of an equipment rack with a specialized cable fixture box and other components such as a PNA-X network analyzer, ECals, power sensors, cables, and adapters. Testing must be performed within this custom test station which are only available at a limited number of Keysight service centers. See Optimized Test Station for more information. |
|
Network analyzer |
N5247B with options:
|
|
Power meter |
N1914A |
|
Power sensor, 3.5 mm |
N8485A |
|
ECal module, Type-N
|
N4690D2 Options 0DC, M0F |
|
ECal module, 3.5 mm
|
N4691D2 Options 0DC, M0F |
|
Barrel adapter, 2.4 mm (f) to Type-N (m)
|
11903D |
|
Barrel adapter, 2.4 mm (f) to 3.5 mm (f)
|
11901B |
|
Adapter, Type-N (f) to 3.5 mm (f)
|
1250-1745 |
|
Cable, 1.85 mm (f) to 1.85 mm (m)
|
|
|
Rigid thru cable |
ET55861-0003 |
|
The power meter used in these procedures will be controlled by the network analyzer through the GPIB connection from the power meter to the network analyzer. Therefore the power meter needs to be added to the Keysight Connection expert via a remote GPIB interface.
The following steps will explain how to configure the PNA and the power meter's remote GPIB interface.
|
|
When using an NI IO card or NI USB-to-GPIB converter, be sure that the NI-VISA Passport for Tulip has been enabled to recognize and detect Keysight hardware. Refer to the following document for more detailed troubleshooting instructions: http://literature.cdn.keysight.com/litweb/pdf/5990-3731EN.pdf |
Ensure that Remote IO Server is enabled on the PNA.
Click on the gear in the upper-right, then select Settings > Remote IO Server options. Ensure Enable Remoter IO Server and Auto-Start Remote IO Servers on Machine Setup are selected.
Close Keysight Connection Expert, and restart the Network Analyzer application by double clicking on the shortcut from the PNA front panel.
Make the GPIB cable connections so that the PNA can control the power meter.
Configure the remote GPIB interface on the PC and in TME.
Click on Test Connection to verify that the connection was made.
In Keysight Connection Expert, you should now see the remote GPIB interface you have created, and the power meter that is connected (by GPIB) to the controller of the PNA.
Now in TME Station Administration, map the power meter to the appropriate board and address. Using the example above, the correct board is 3 and the address is 13.
This procedure performs CAL ALL on multiple frequency sweep channels with different source attenuation on the network analyzer.
Click on the links below for connection setup images. To expand all, click the Expand All button
in the toolbar (webhelp only).
Click here for power sensor calibration.
Click here for power calibration.
Click here for adapter characterization. This step does not apply to 3.5 mm models: N9918B and N9938B with Option 100.
Click here for s-parameter calibration.
Click here for s-parameter calibration verification.
Click here for verification power sensor calibration.
Click here for power verification.
This procedure performs CAL ALL on multiple power sweep channels with different source and receiver attenuation on the network analyzer.
Click on the links below for connection setup images. To expand all, click the Expand All button
in the toolbar (webhelp only).
Click here for power sensor calibration.
Click here for power calibration.
Click here for adapter characterization. This step does not apply to 3.5 mm models: N9918B and N9938B with Option 100.
Click here for s-parameter calibration.
Click here for s-parameter calibration verification.