|
|
Some FieldFox model and option combinations will require the installation of the CFG Option in order to complete utilities. Refer to the CFG Option section for more information. |
The utilities provided in this menu are not intended to be run as part of an annual calibration. These utilities are intended to be used for troubleshooting or repair purposes. (The exception to this are the first four network analyzer calibration utilities which are required to calibrate the network analyzer used in some tests and adjustments.)
Each completed utility is labeled Complete or Fail. Some utilities produce a text file that may be useful when troubleshooting problems.
Following are the utilities available for the FieldFox handheld analyzers:
|
Name |
Comments |
|
|
1. |
Network Analyzer Frequency Sweep Calibration |
|
|
2. |
Network Analyzer Power Sweep Calibration |
|
|
3. |
N995xA and N996xA |
|
|
4. |
N995xA and N996xA |
|
|
5. |
Applies to all models and options except for the N991xB and N993xB. |
|
|
6. |
N9912A, N9923A only |
|
|
7. |
Applies to all models |
|
|
8. |
N991xA with Option 233 (not for N9912A) N993xA N995xA with Option 233 N996xA |
|
|
9. |
Applies to all models and options (except for N9912A and N9923A) |
|