Overview of Required Test Equipment

The test equipment that is required for performance verification is different for each PNA model family.

Select from the following list:

For a list of equipment required for a specific test, see the applicable test description in the Performance Tests section.

Equipment Lists for Test Stations

Generally, a single piece of equipment should not be entered multiple places in the equipment list for a given test station under TME. For instance, when a test station requires two power-sensor cables, two separate cables must be used. Mechanical calibration kits are an exception to this rule. When a test station lists two calibration kits, a single mechanical calibration kit may be used.