Performance Tests Overview

This section lists the available performance tests for the PNA series network analyzers. Perform the tests in the order shown to minimize connection changes and to avoid recalibration of the power sensor.

Test Order for PNA:

  1. Operator's Check

  2. Source Power Accuracy a

  3. Source Maximum Power a

  4. Source Power Linearity

  5. Frequency Accuracy

  6. Trace Noise

  7. Receiver Compression a

  8. Noise Floor a

  9. Calibration Coefficients

  10. System Crosstalk

  11. Dynamic Accuracy b, c

Footnotes:

  1. Since three power sensors are required for frequency range above 50 GHz, the following tests are divided in TME to avoid unnecessary recalibration of the power sensors:
  2. If a Dynamic Accuracy Test Set is used, an additional 30-minute wait can be avoided at the start of the test by connecting the power sensor to the test set at the completion of the Noise Floor test.

  3. The test solution depends on the mapped test equipment. Refer to the test topic pages for more information.