Test Equipment Overview

This section lists the test equipment needed to run performance tests and adjustments for PXIe signal analyzers. Models for each test equipment category are given in order of preference. Alternate models are also listed but should be considered a lower priority. Model numbers are Keysight, Agilent, or HP unless otherwise specified.

Refer to each individual test for specific setup configurations with required cables and adapters. The computer and all test equipment are connected to the device under test (DUT) using GPIB and PXIe.

Click on the link below for the required test equipment for your PXIe signal analyzer model: