The performance verification tests are designed to provide the highest level of confidence that the instrument being tested conforms to the published, factory-set specifications. The tests are designed to test an instrument operating within the temperature range defined by the instrument specifications.
Calibrated ETE should be stored for a minimum of two hours within the full temperature range. The DUT should have a 45 minute warmup cycle prior to testing.
|
|
|
Each test will check at the beginning and at the end of the test that modules are not exceeding the maximum module temperature specification for that test. A warning will be given to the user if a module temperature is exceeded. Refer to the Recommended Practices for Module/Chassis Temperature Control for more information.
The recommended calibration cycle is every 12 months. Performance tests are listed in the order that they should be performed. Click on the link below for the test list for your PXIe signal analyzer model.
click here:
click here: