N7872A Adjustments Overview

  • Running an adjustment will invalidate the calibration date of that module as well as the calibration information for all PXIe systems that the module belongs to.

  • At the start of each adjustment, the user may experience a delay of up to two minutes as the application initializes and gathers information to run the adjustment. This is normal behavior.

  • The digitizer, synthesizer, and downconverter modules must be within one trigger bus (slot 1-6, slot 7-12, or slot 13-18). If they are not, then the trigger busses must connected. It is highly recommended to install the modules in slots 2-6. The M9300A frequency reference module must be installed in slot 10 of the chassis.

  • In all test equipment configurations, cables and adapters must be properly torqued. Exceeding recommended torque values can cause damage to a cable or adapter which may produce inaccurate test results.

Adjustments for the PXIe signal analyzer instruments are module-level adjustments. Adjustments for the M9300A frequency reference module are supported by the separate calibration application N7873A.

Never perform adjustments as routine maintenance. Adjustments should be performed only after a repair or performance test failure. If any performance test fails, do the following:

List of Adjustments

For M9391A adjustments, Closedclick here:

 

For M9393A adjustments, Closedclick here: