| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Sub ConfigureCrossCorrelatedEvm( _ ByVal ccIndex As Integer _ ) | |
Parameters
- ccIndex
- Index of the ComponentCarrier whose settings to keep.
| Exception | Description |
|---|---|
| System.ArgumentOutOfRangeException | ccIndex is not a valid ComponentCarrier index. |
| System.InvalidOperationException | The measurement has an odd number of measurement channels, has fewer than two measurement channels, or the acquisition is sequential. |
Cross-Correlated EVM measures the same signal through multiple input channels to reduce the input channels' own EVM contribution. This keeps only the ComponentCarrier specified by ccIndex, duplicates it into two cross-correlation groups, and assigns each group one contiguous half of the measurement channels (the first half to the first group, the second half to the second), then enables Cross-Correlated EVM. It requires an even number of measurement channels (two or more) and does not support sequential acquisition. Two channels form single-channel groups; four or more channels form MIMO cross-correlation groups.
All other ComponentCarriers are removed from ComponentCarriers, and DisplayedCarrierIndex is set to 0.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)