Keysight 89600 VSA .NET API
Create() Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MeasurementCollection Class > Create Method : Create() Method


Glossary Item Box

Creates a new vector measurement.

Syntax

Visual Basic (Declaration) 
Public Overloads MustOverride Function Create() As Measurement
C# 
public abstract Measurement Create()
C++/CLI 
public:
abstract Measurement^ Create(); 

Return Value

A handle to the new measurement.

Remarks

Multiple measurements are not supported prior to release 15.0 of the Keysight 89600 VSA software.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also