| Overload | Description |
|---|---|
| Create() | Creates a new vector measurement. |
| Create(String) | Creates a new vector measurement. |
| Create(Type) | Creates a new measurement of the specified type. |
| Create(Type,String) | Creates a new measurement of the specified type with the supplied name. |
| Create(Measurement) | Creates a new measurement identical to the supplied measurement. |
| Create(Measurement,String) | Creates a new measurement identical to the supplied measurement. |
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)