| Visual Basic (Declaration) | |
|---|---|
Public Overloads Overridable Function Create( _ ByVal originalMeasurement As Measurement _ ) As Measurement | |
| C# | |
|---|---|
public virtual Measurement Create( Measurement originalMeasurement ) | |
| C++/CLI | |
|---|---|
public: virtual Measurement^ Create( Measurement^ originalMeasurement ) | |
Parameters
- originalMeasurement
- The measurement to be duplicated.
Return Value
A handle to the new measurement.| Exception | Description |
|---|---|
| System.ArgumentException | Is raised if originalMeasurement is not a current, valid measurement. |
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 15.0