Keysight 89600 VSA .NET API
Create(Measurement,String) Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MeasurementCollection Class > Create Method : Create(Measurement,String) Method


originalMeasurement
The measurement to be duplicated.
name
The name to assign to the new measurement.

Glossary Item Box

Creates a new measurement identical to the supplied measurement.

Syntax

Visual Basic (Declaration) 
Public Overloads Overridable Function Create( _
   ByVal originalMeasurement As Measurement, _
   ByVal name As String _
) As Measurement
C# 
public virtual Measurement Create( 
   Measurement originalMeasurement,
   string name
)
C++/CLI 
public:
virtual Measurement^ Create( 
   Measurement^ originalMeasurement,
   String^ name
) 

Parameters

originalMeasurement
The measurement to be duplicated.
name
The name to assign to the new measurement.

Return Value

A handle to the new measurement.

Exceptions

ExceptionDescription
System.ArgumentExceptionIs raised if originalMeasurement is not a current, valid measurement.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 15.0

See Also