Keysight 89600 VSA .NET API
IsCalculateMeasurementData(String,Boolean) Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class > IsCalculateMeasurementData Method : IsCalculateMeasurementData(String,Boolean) Method


dataName
The data name.
isCalculate
Whether the measurement data is calculated.

Glossary Item Box

Set whether the passed measurement data is calculated even if not displayed.

Syntax

Visual Basic (Declaration) 
Public Overloads MustOverride Sub IsCalculateMeasurementData( _
   ByVal dataName As String, _
   ByVal isCalculate As Boolean _
) 
C# 
public abstract void IsCalculateMeasurementData( 
   string dataName,
   bool isCalculate
)
C++/CLI 
public:
abstract void IsCalculateMeasurementData( 
   String^ dataName,
   bool isCalculate
) 

Parameters

dataName
The data name.
isCalculate
Whether the measurement data is calculated.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also