Occurs when secondary information about a property, such as limits, changes.
Syntax
Event Data
The event handler receives an argument of type PropertyInfoChangedEventArgs containing data related to this event. The following PropertyInfoChangedEventArgs properties provide information specific to this event.
| Property | Description |
|---|
| PropertyName | Gets the name of the property whose information has changed. |
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 14.00
See Also