| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property Center As Double | |
| C# | |
|---|---|
public abstract double Center {get; set;} | |
You can set the frequency range with the Center and Span properties, or with the StartFrequency and StopFrequency properties. You can also use the SetCenterSpan or SetStartStopFrequency methods to set the frequency range all at one time.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)